cancel
Showing results for 
Search instead for 
Did you mean: 

FTP Client on STM32

hpipon957
Associate III
Posted on January 07, 2012 at 22:09

Hi All

The following new video shows a demonstration of embedded FTP client operation in the uTasker project:

http://youtu.be/sZOCFLDfGTk

It is not shown running on an STM32 board in the demo but it is now included in the uTasker STM32 project as detailed here:

http://www.utasker.com/forum/index.php?topic=1697.0

It is therefore operational on STM32F1, STM32F2 and STM32F4 evaluation boards using GCC, Rowley Crossworks, ATOLLIC TrueStudio, IAR or Keil uVision, as well as in real-time simulation in VisualStudio 6 or VisualStudio 20xx.

The FTP client user's manual is available at

http://www.utasker.com/docs/uTasker/uTaskerFTP_client.pdf

Regards

Mark

#utasker-stm32-ftp-client
1 REPLY 1
amin23
Associate II
Posted on January 09, 2012 at 09:00

Very interesting.