2015-07-06 11:17 AM
I am working with STM32F427ZIT6 (Keil MDK-ARM 5.15) and want to implement a delay function based on Timer 6 in a single pulse mode. The delay function is:
void Delay_us(uint16_t amt_us)
{
TIM6->CNT = 0;
TIM6->ARR = amt_us;
/* start timer and monitor update flag */
TIM6->CR1 |= 0x0001;
while ((TIM6->SR & 0x0001) == 0) {;}
TIM6->SR &= 0xFFFE; /* clear update flag */
/* timer stops */
} /* end Delay_us() */
Timer 6 initialization code is exported from STM32CubeMX:
/* TIM6 init function */
void MX_TIM6_Init(void)
{
TIM_MasterConfigTypeDef sMasterConfig;
htim6.Instance = TIM6;
//HAL_TIM_Base_Init(&htim6);
htim6.Init.Prescaler = 83; //168;
htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
htim6.Init.Period = 0;
HAL_TIM_Base_Init(&htim6);
HAL_TIM_OnePulse_Init(&htim6, TIM_OPMODE_SINGLE);
// sMasterConfig.MasterOutputTrigger = TIM_TRGO_ENABLE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig);
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_ENABLE; is commented out since I don't need a trigger output.
I also tried to use the ''old way'' initialization I always used with M3:
void TIM6_Init(void)
{
__TIM6_CLK_ENABLE();
/* prescaler register is loaded with value for Fcnt = 1 MHz at 84 MHz */
TIM6->PSC = 83;
/* timer is used as upcounter (DIR=0) in one-pulse mode (OPM=1), */
/* only overflow generates an update event (URS=1), */
/* update event is generated, no interrupt */
TIM6->CR1 = 0x000C;
}
The only thing I have in a main loop is toggling of an output pin with a delay:
while (1)
{
/* toggle PB12 (TEST1) at 10 ms */
Delay_us(10000);
cnt++;
GPIOB->ODR ^= 0x1000;
}
Variable
cntshows how many times the loop was executed.
When I debug the program, it goes into Hard Fault after executing a loop a few times (I saw
cnt equal to 1, 2, 81 etc. - no certain value.
If I replace the call to the Delay_us() by the simple delay loop (delay value is not important)
for (uint32_t i = 0; i < 1000000; i++) {;}
no Hard Fault exception is generated.
What can cause such behavior? I used this method many times with multiple M3s and never had any problems.
Thank you for advice,
Gennady
2015-07-06 11:26 AM
What can cause such behavior?
An interrupt without a service routine? Touching the wrong area of memory? Does the Hard Fault seem to identify with an interrupt, or specific instructions in your code?2015-07-06 11:38 AM
No interrupt is enabled for a timer. I am just polling the Update interrupt flag.
I haven't tried to further debug the Hard Fault, thought that may be there is a simple answer to my problem. Seems like I will need to do that :-(.2015-07-06 12:30 PM
Is this your own hardware, or a DISCOVERY/EVAL board?
Any other hardware initialized? What is the clock source? JW2015-07-06 12:36 PM
It's our own board.
At this point only Timer 6 and GPIOs are initialized.Clock source is HSE.Gennady2015-07-06 06:16 PM
2015-07-07 08:50 PM
Seems like it has nothing to do with the Cube. I've made another project with the same functionality based on RTE - same behavior.
Nevertheless I've found that reason for a hard fault is IBUSERR. Stack pointer changes from regular 0x2000818 to 0x180007C8, what is invalid memory area.But I still don't understand what is causing it and how it's related to operations on timer registers.Another hint - when I load program to the flash, it sometimes works, sometimes doesn't. But it NEVER works after cycling power. Also I've noticed that PDR_ON pin is not connected to VCC, so power supply supervisor is not enabled. Don't know if it may have any connection with the problem.2015-07-09 12:13 PM
Resolved. As I mentioned earlier, the PDR_ON pin was not connected, thus disabling power supply supervisor. Also, capacitors vcap1 and vcap2 were not in place, so even when PDR_ON was connected to VDD, the power supply supervisor didn't operate properly, I guess messing up initialization.
When this issues were corrected, the problem in discussion disappeared.Thanks to everybody who tried to help me,Gennady