cancel
Showing results for 
Search instead for 
Did you mean: 

Difference between Low/medium/high density devices and conectivity line devices

waldin80
Associate II
Posted on July 28, 2010 at 08:57

Difference between Low/medium/high density devices and conectivity line devices

4 REPLIES 4
stforum2
Associate II
Posted on May 17, 2011 at 14:00

A brief description of each sub-family is listed here:

http://www.st.com/mcu/familiesdocs-110.html#Datasheet

but if you really want to know the detailed differences then you need to download each datasheet.

The 'density' directly relates to the amount of flash memory.

'connectivity line' has an OTG USB interface, dual CAN interfaces and ethernet

'performance line' has CAN and USB (device)

'USB access line' has USB but no CAN

'access line' has neither USB or CAN

'value line' has an HDMI interface

Hope this helps.

waldin80
Associate II
Posted on May 17, 2011 at 14:00

Thks for replying:

My doubt is, what kind of type of device I have?

I´m programming STM32F103VE.

Is it High density device or Connectivity device?

Both groups of devices have diferent clock tree (see RM0008 pag 77 and 107), that is my doubt

waldin80
Associate II
Posted on May 17, 2011 at 14:00

Ok, Thks for the help. Ten points for you 0690X0000060MlFQAU.gif

stforum2
Associate II
Posted on May 17, 2011 at 14:00

You have a high density performance device with 512k of flash and 64k of RAM.

14611.pdf describes your device.

Connectivity devices are ...105... and ...107...