cancel
Showing results for 
Search instead for 
Did you mean: 

EXTERNAL TRIGGER ADC

gdiez
Associate II
Posted on September 06, 2010 at 13:07

EXTERNAL TRIGGER ADC

5 REPLIES 5
Posted on May 17, 2011 at 14:05

Don't see code setting up the base vector address.

Don't see code setting up the NVIC priority group.

See code using the same sub/priority more than once.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
lipin
Associate II
Posted on May 17, 2011 at 14:05

I don’treally understand why do you want measure conversion time it is deterministic.I guess you are looking for TIM_ITConfig(TIM1, TIM_IT_Update, ENABLE). 

From wantI remember you want to create pwm signal based on analog value. Use one of CCmode flags to fire ADC at the end of pwm cycle then compute duty either by theend of conversion or at tim update event and use other CC register to generatepwm signal. There is going to be a bit of cycles lost for calculations. If youwant to make it precise use CYCCNT register to measure execution time andadjust CC accordingly. Personally I would use adc continuous mode and stop worryingabout triggering etc for the sake of simplicity.

Regards

Thomas

gdiez
Associate II
Posted on May 17, 2011 at 14:05

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6ZR&d=%2Fa%2F0X0000000bqv%2FqVySHmPZF.oKIGRuDOcSil1V48xe1Z2eZwICFLwdy3g&asPdf=false
gdiez
Associate II
Posted on May 17, 2011 at 14:05

Hi my friend:

That´s my next target. Get in oscilloscope, the ADC conversion time, with a led toggle.

I´ve achieved my old target like that:

 

Configure TIM1 like PWM1 and like the trigger of adc

void TIMER_configuration(void)

  TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

  TIM_OCInitTypeDef  TIM_OCInitStructure; 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ TIM1 y TIM3 CLK ~~~ */ 

  /* TIM 1 CAPTURE-COMPARE-PWM MODE */

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 ,ENABLE);   /* RCC_APB2ENR.TIM1EN ENABLE CLK TIM1 */

  RCC_APB2PeriphResetCmd(RCC_APB2Periph_TIM1 ,DISABLE);  /* RCC_APB2RSTR.TIM1RST RESET TIM1 */

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ CONFIGURACION TIM3 PARA TRIGGER ADC ~~ */

  /* ~~~~~~~ CONFIGURACION PARA 20KHz ~~~~~~~~~~~~~~~~~~~~ */

  #define Prescala 1      /* Maximo 65536 */

  #define Periodo 2799    /* Maximo 65536 */

  TIM_TimeBaseStructure.TIM_Prescaler = Prescala-1;             /* DIVIDE EL CK_CNT=CK_PSC/(TIMx_PSC+1) - TIMx_PSC */

  TIM_TimeBaseStructure.TIM_Period = Periodo;                   /* NUMERO DE PULSOS A CONTAR DE CK_CNT - PERIODO TIMx_ARR */

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Down; /* MODO DE CONTADOR - TIM_CR1.DIR */

  TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;       /* PARA FILTROS DIGITALES - TIM_CR1.CKD */

  TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;              /* TIM_RCR */

  TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ CONFIGURACION TIM1 TRGO TRIGGER ~~ */  

  TIM_SelectOutputTrigger(TIM1,TIM_TRGOSource_Update); 

 

  TIM1_ClearITPendingBit(TIM1_FLAG_Trigger);            /* BORRA UPDATE INTERRUPT BIT TIMx_SR.UIF */ 

  TIM_ITConfig(TIM1, TIM_IT_COM, ENABLE);

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~PWM1 Mode configuration: Channel2 ~~ */

  /* PWM1 Mode configuration: Channel2 */

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;   /* ELIGE EL MODO PWM */

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 0;                            /* Duty Cycle */

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  TIM_OC2Init(TIM1, &TIM_OCInitStructure);

  TIM_CtrlPWMOutputs(TIM1, ENABLE);                /* TIM1 Main Output Enable */ 

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ 

  TIM_Cmd(TIM1,ENABLE);                                     /* ENCENDIDO TIM1 */ 

}

Configure the ADC with a external trigger

 

void ADC_configuration(void)

{

  ADC_InitTypeDef ADC_InitStructure;

  ADC_DeInit(ADC1);               /* Inicializa los registros */

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */  

  /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ ADC1 clock ~~~~~~~~~~~ */ 

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 , ENABLE);

  /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ CONFIGURACION DEL ADC1 ~~ */ 

  ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;                     /* ELIGE EL MODO DE OPERACION - ADC_CR1.DUALMOD */

  ADC_InitStructure.ADC_ScanConvMode = ENABLE;                           /* HABILITA MODO SCAN (GRUPO DE CANALES) - ADC_CR1.SCAN */

  ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;                     /* DESHABILITA EL MODO CONTINUO - ADC_CR2.CONT */

  ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigInjecConv_T1_TRGO; /* HABILITA TRIGGER POR TIMER3 - ADC_CR2.EXTSEL */

  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;                 /* ALINEACION A LA DERECHA - ADC_CR2.ALIGN */

  ADC_InitStructure.ADC_NbrOfChannel = 1;                                /* NUMERO DE CANALES DEL GRUPO */

  ADC_Init(ADC1, &ADC_InitStructure);

  /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ CONFIGURACION DEL ADC1 ~~ */

/* SELECCION DEL SAMPLE TIME - ADC_SMPR2.SMPx, SELECCION SECUENCIA INJECTED - ADC_SQR1 */

/* ~~~~~~~~~~~~~~~~~~ ADC conversion Time = Sampling Time + 12,5 cycles ~~~~~ */ 

  ADC_InjectedChannelConfig(ADC1, ADC_Channel_15, 1, ADC_SampleTime_1Cycles5);

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ HABILITACION DEL ADC1 DMA */

//  ADC_DMACmd(ADC1, ENABLE);                      /* HABILITACION DIRECT MEMORY ACCESS MODE - ADC_CR2.DMA */

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ HABILITACION DEL ADC1 ~~~ */

  ADC_Cmd(ADC1, ENABLE);                   /* DESPIERTA AL ADC - ADC_CR2.ADON */

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ RESETEO DEL ADC1 ~~~~~~~ */

  ADC_ResetCalibration(ADC1);     /* INICIALIZA REGS. CALIBRACION - ADC_CR2.RSTCAL */        

  while(ADC_GetResetCalibrationStatus(ADC1)); /* FIN CALIBRACION REGS. - ADC_CR2.RSTCAL=0 */

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ CALIBRACION DEL ADC1 ~~~ */

  ADC_StartCalibration(ADC1);         /* COMIENZA LA CALIBRACION SELECCIONADA */

  while(ADC_GetCalibrationStatus(ADC1));    /* CALIBRACION COMPLETADA - ADC_CR2.CAL=0 */

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~ CONFIGURACION DE LA INTERRUPCION EOC DEL ADC1 ~~~ */ 

  ADC_ClearITPendingBit(ADC1,ADC_IT_JEOC);        /* BORRA JEOC bit ADC1_SR.EOC */ 

  ADC_ITConfig(ADC1,ADC_IT_JEOC,ENABLE);       /* HABILITA LA INTERRUPCION EOC */

 

/* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */  

  ADC_ExternalTrigInjectedConvCmd(ADC1, ENABLE);

 

}

gdiez
Associate II
Posted on May 17, 2011 at 14:05

My next target is the follow. I want to be able to see in oscilloscope the ADC Time conversion

1.- Start the ADC conversion, and toggle one pin (I think watching the TIM1 ISR (I cant at this moment)).

2.- Toggle this pin another time when the conversion finishes (Watching ADC ISR, I can do this).

3.- Get the time with the oscilloscope. By this way i will have the ADC TiME conversion. My boss told me that he wants to see it in my oscilloscope.

0690X00000602P7QAI.bmp