cancel
Showing results for 
Search instead for 
Did you mean: 

Adding files from other folders

carnett1
Associate II
Posted on December 09, 2010 at 17:22

I have a terminal program up and running.  I am messing arournd with changing TIM3 output on channel 2.  Everything is going well.  However when I try to use TIM2 I don't have the right prototype in stm8s_tim2.c or .h so i add those files from a different project folder but it doesn't seem to recognize them.  I find TIM8_Cmd in both the tim2.c and .h files but the compiler  says they are not there.  I am using the Comic tool.  Is there a problem with adding files in the project inside the STVD that are n;ot in the same folder?

charles

0 REPLIES 0