2010-10-26 04:07 AM
hi.
i cant understand why EOC wont go up to ''1'' after conversion. i can see the result in ADC->DR but the flag wont go up. why? thanks. #include ''stm32F10x.h'' #define CCR_ENABLE_Set ((uint32_t)0x00000001) void setsystemclock(void); __IO uint16_t ADCConvertedValue; int temp=0; int main(void) { setsystemclock(); //set system clock to 24Mhz3 //rcc CONFIGURATION RCC->AHBENR=RCC_AHBENR_DMA1EN; //dma clock enable RCC->APB2ENR=RCC_APB2ENR_IOPCEN | RCC_APB2ENR_ADC1EN; //portc and ADC clock enable. //GPIO CONFIGURATION GPIOC->CRL=0x0;// ADC1_IN14 //ADC configuration ADC1->CR1=ADC_CR1_SCAN; ADC1->CR2=ADC_CR2_ALIGN | ADC_CR2_EXTSEL;// |ADC_CR2_DMA ; //data align right , software start ADC1->SMPR1=0;// 1.5 cycles conversion time ADC1->SQR3=0xe;//channel number 14 PC4 first conversion //ADC1->CR2 |=ADC_CR1_SCAN ; /* Enable ADC1 DMA */ ADC1->CR2 |=ADC_CR2_ADON; /* Enable ADC1 */ ADC1->CR2 |=ADC_CR2_RSTCAL ;//reset calibration while ((ADC1->CR2 & ADC_CR2_RSTCAL) != 0x00); //wait for end of ADC1 reset calibration register ADC1->CR2 |=ADC_CR2_CAL;/* Start ADC1 calibaration */ while((ADC1->CR2 & ADC_CR2_CAL) != 0x00);/* Check the end of ADC1 calibration */ ADC1->CR2 |=ADC_CR2_SWSTART |ADC_CR2_EXTTRIG; /* Start ADC1 Software Conversion */ while(1) { temp=ADC1->SR+1; if((temp&ADC_SR_EOC)>0) { temp=ADC1->DR; ADC1->CR2 |=ADC_CR2_SWSTART |ADC_CR2_EXTTRIG; temp=temp+1; } } } void setsystemclock(void) { RCC->CR |= RCC_CR_HSEON; // Wait until it's ready while ((RCC->CR & RCC_CR_HSERDY) == 0) ; // Select PREDIV1 as PLL source and sett PLL mul to 3 (set bit 0) // for 8*3 = 24 MHz RCC->CFGR |= RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL_0; // Start PLL RCC->CR |= RCC_CR_PLLON; // Wait until it's ready while ((RCC->CR & RCC_CR_PLLRDY) == 0) ; // Select PLL as system clock RCC->CFGR |= RCC_CFGR_SW_PLL; // Here we can check if PLL is used, and maybe disable HSI // Disable HSI RCC->CR &= ~RCC_CR_HSION; RCC->CFGR|=RCC_CFGR_MCO_2; //sys clock output }2010-10-26 11:33 PM
2010-12-28 10:44 AM
Hi be_senyor.ezra,
I hope it is not too late to give you an answer 😉 I think that the problem of your code is here: '' if((temp&ADC_SR_EOC)>0) { temp=ADC1->DR; ADC1->CR2 |=ADC_CR2_SWSTART |ADC_CR2_EXTTRIG; temp=temp+1; } '' when the '' if'' condition arrives, the program reads what the ADC's DataRegister contains but, at the same time, it erases and put to zero the flag of EOC!!! For more info read the Reference Manual RM0008 on the STM32F10x MCU family (page 219). Let me know if you have found a remedy to your problem! Greetings Massimo