2016-01-29 08:41 AM
Hi everybody,
this is to inform all of you that a new FW for SPWF01Sx, named 3.5, has just been released.It includes new features...:- AT+S.RMPEER- AT+S.HTTPREQ (thanks to Flow forum user)- AT+S.FSR- AT+S.HTTPDFSWRITE (thanks to burton.mark forum user)- etf_mode var- console1_delimiter var (thanks to coghlin.patrick forum user)- dhcp_lease_time var- dns_mode var- use_cgis var- use_ssis var- use_decoder var- wifi_region (thanks to elia.marco.002 forum user)...and bug fixing:- automatic deletion of RAM files with the same name- hidden AP (thanks to Joe forum user)- decoding function to firstset/output_demo (thanks to Flow forum user)- UART overrun (thanks to siebke.georg forum user)It's still not on the website, but you can contact your ST contact/distributor...Feel free to comment.Best regardsjerry2016-01-31 10:32 PM
Edit:
I've updatet my modules. Is there also an update of the user manual available? Hi Jerry, great news!!! Thank you very much in advance for the new features. I will try to get the Firmware from my distri and test the new features. Cheers, Flow2016-02-02 11:04 PM
Hi Flow,
user manuals, application notes, and hands on are going to be published on the website in a few days.In the meantime you can use the HELP command, or ask here 🙂Regardsj2016-02-02 11:30 PM
Hi Jerry,
thank you. I already tried the help function 😉 I will wait... and ask here 😉 Regards, Flo2016-03-22 04:12 AM
Hi,
where can I download the hands on WiFi firmware? STSW-IDW001, STSW-IDW001 pages does not contain any valid donwload link...thanks.2016-03-24 08:17 AM
2016-05-30 07:27 AM
Hi,
I update the module and I'm trying to use the ''httpreq'' command, but without any success.I notice that if I put a comma before the port number (a third one as described in the manual) the module report an ERROR (missing argument). If I don't put the third comma (with or without the port number) the module crash and I have to reset it (with the switch, serial command are useless). In this scenario, I enabled the localecho1 and I don't see, in the echo, the command data but only the first part of the command (until the \r).At the moment I'm trying to replicate a simple get (the same sent with the at+s.httpget command) so I can understand how that command works.There are any examples for this command or any more explanations than those in the manual?Thanks for the help.Tommaso2016-06-09 12:48 AM
Hi Tommaso,
here (https://my.st.com/public/STe2ecommunities/interface/Lists/WiFi%20Modules/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2finterface%2fLists%2fWiFi%20Modules%2fHTTPPOST%20Example%20Android%20GCM&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800086789498A6852D4897EA192EB1DEE909&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Finterface%2FLists%2FWiFi%2520Modules%2FAllItems.aspx¤tviews=476) a discussion on httpreq command. Basically, you need to format a packet containing the request, and use its length as command parameter. Do not forget to insert ''\r\n\r\n'' at the end of the packet. About the crash, can I have the command used? This way, I can push to fix it. Regards jerry2016-06-10 02:04 AM
Hi,
This is the command I was sending: at+s.httpreq=192.168.1.174,80,66\rGET / op.php HTTP/1.1\r\nUser-Agent: SPWF01SA1\r\nConnection: close\r\n\r\n\rI was waiting the same response sending the ''at+s.httpget=192.168.1.174,op.php\r\n\r'' command (this second command is correctly working and I got the 200 response from the server).Actually I find the problem: it seems the SPWF10S needs a ''pause'' between the command and the data:at+s.httpreq=192.168.1.174,80,66\rGET / op.php HTTP/1.1\r\nUser-Agent: SPWF01SA1\r\nConnection: close\r\n\r\n\rAt the moment I'm sending the 2 strings manually, but it should be appropriate for ST to specify the minimum time between them, otherwise (e.g. the previous case with a single string) the SPWF10S crashes (don't accept any command and needs a manual reset).Now I think to have the same problem mentioned in the discussion you linked. Using the httpreq command I got a 400 response from the server.Furthermore it seems the PORT must be specified: if it is not, as described in the manual, the SPWF10S replay with ''ERROR: connect() failed, aborting''.Regards,Tommaso2016-06-10 03:28 AM
Tommaso,
there is no need to ''pause'' between the command and the data. This is what I see from a windows utility running on PC (it's called docklight):at+s.httpreq=www.wikipedia.com,80,370<CR>
GET /wiki.com/Pagina_principale HTTP/1.1 <CR><LF>Connection: Keep-Alive<CR><LF>User-Agent: Mozilla/5.0 (compatible; Konqueror/3.2; Linux) (KHTML, like Gecko)<CR><LF>Accept: text/html, image/jpeg, image/png, text/*, image/*, */*<CR><LF>Accept-Encoding: x-gzip, x-deflate, gzip, deflate, identity<CR><LF>Accept-Charset: iso-8859-1, utf-8;q=0.5, *;q=0.5 <CR><LF>Accept-Language: en<CR><LF>Host: it.wikipedia.org<CR><LF><CR><LF>10-Jun-16 12:21:56 [RX] - HTTP/1.1 301 TLS Redirect<CR><LF>Server: Varnish<CR><LF>Location: https://it.wikipedia.org/wiki.com/Pagina_principale<CR><LF>;Content-Length: 0<CR><LF>Accept-Ranges: bytes<CR><LF>Date: Fri, 10 Jun 2016 10:21:56 GMT<CR><LF>X-Varnish: 888050924<CR><LF>Age: 0<CR><LF>Via: 1.1 varnish<CR><LF>Connection: close<CR><LF>X-Cache: cp3041 int<CR><LF>Set-Cookie: WMF-Last-Access=10-Jun-2016;Path=/;HttpOnly;secure;Expires=Tue, 12 Jul 2016 00:00:00 GMT<CR><LF>X-Client-IP: 62.110.21.125<CR><LF>Set-Cookie: GeoIP=IT:09:Baranzate:45.53:9.12:v4; Path=/; secure; Domain=.wikipedia.org<CR><LF><CR><LF><CR><LF><SUB><SUB><SUB><CR><LF><CR><LF>OK<CR><LF>Are you providing this command to the module by exteranal MCU?About the fault, probably you are running this command leaving the comma inside it:- at+s.httpreq=www.wikipedia.com,80,370 -> ok- at+s.httpreq=www.wikipedia.com,370 -> ok- at+s.httpreq=www.wikipedia.com,0,370 -> error- at+s.httpreq=www.wikipedia.com,,370 -> error (comma must not be added)