cancel
Showing results for 
Search instead for 
Did you mean: 

c++ code sample

federicomanfrin
Associate II
Posted on October 15, 2010 at 13:30

Hi, I'm going to try to write a few c++ sample projects.

I'd like to use the ST demo board as target board.

Is it possible to download some C++ project sample?

Thanks

Federico

1 REPLY 1
Posted on October 15, 2010 at 14:53

I'm going to try to write a few c++ sample projects. I'd like to use the ST demo board as target board.

 

 

Is it possible to download some C++ project sample?

 

I don't think C++, and it's code size and runtime overhead is wholly appropriate for embedded micro controller work. For example C code, follow the link printed on the board and download the firmware library source which includes the library and sample/example projects.

Would also suggest downloading the demo Keil or IAR tool chains.

http://www.st.com/mcu/contentid-133-110-STM32VLDISCOVERY.html

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..