cancel
Showing results for 
Search instead for 
Did you mean: 

[bug] STM32CubeMX 4.23.0 does not copy startup.s

Jan Breuer
Associate III
Posted on November 14, 2017 at 09:44

I have selected option for 'STM32 Firmware Library package' -> 'copy only the necessery library files'.

I'm using just LL libraries and GPDSC project.

All files ware generated without error but no startup file was present in the project, only blank directories 'arm', 'gcc' and 'iar' ware created in directory 'Drivers/CMSIS/Device/ST/STM32F0xx/Source/Templates/'

On the other hand, it copies 'system_stm32f0xx.c' in 'Templates' directory, which is not needed, because similar file is generated with the same name and functionality to the 'Src' directory. 

MCU: STM32F030F4Px

PC OS: Linux

CubeMX version: 4.23.0

Firmware package: STM32Cube FW_F0 V1.9.0

1 REPLY 1
Imen.D
ST Employee
Posted on November 15, 2017 at 14:46

Hello,

Your issue is raised to CubeMx team for further check and investigation.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen