cancel
Showing results for 
Search instead for 
Did you mean: 

CAN device under uCLinux

christopher23
Associate II
Posted on November 04, 2010 at 12:49

CAN device under uCLinux

1 REPLY 1
christopher23
Associate II
Posted on May 17, 2011 at 14:13

success...i get it compiled now and i think all dependecies are right but when i run it on the board i get the following error:

CPU: 0    Not tainted  (2.6.26-uc0 #21)

pc : [<680a9952>]    lr : [<680a9f47>]    psr: 61000000

sp : 680aff58  ip : 00000000  fp : 00000000

r10: 680ab9b8  r9 : 00000000  r8 : 680aa029

r7 : 680ab8b9  r6 : 00000001  r5 : 680affa8  r4 : 00000001

r3 : e000ed00  r2 : 680affb0  r1 : 680affa8  r0 : 05fa0700

what does this want to say to me? and how can i solve that problem?

thanks

christopher