cancel
Showing results for 
Search instead for 
Did you mean: 

GUI Builder

oe2
Associate III
Posted on March 04, 2015 at 08:03

Have someone used ST GUI Lib together with displays of 800x480?

When I start GUI builder, and select this resolution only a part of my new screen is shown. Does anyone have any idea??

Have someone used this Lib with ssd1963?

If so, do anyone know if there are som good code to start Writing HAL from?

#ssd1963-gui-800x480
1 REPLY 1
ken4ward
Associate
Posted on March 04, 2015 at 10:07

Thanks. Though I'm sure I'm not posting on the right thread, pardon me. This is my first day on this forum. I've searched roughly to download SPIRIT1 SDK suite with no success, can someone help me post the link of where to download it from.