cancel
Showing results for 
Search instead for 
Did you mean: 

How to Add A Linked File Resource in System Workbench for STM32?

Martin.Sergio
Associate III
Posted on October 05, 2017 at 08:25

Hi,

I´m using a STM32F469I_Eval and in the Examples provides with STM32Cube_FW_F4, I can see that there are some Linked Resources (FILES). If I edit the .project file there are something like that:

<link>

<name>Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal.c</name>

<type>1</type>

<locationURI> copy_PARENT1/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal.c</locationURI>

</link>

<link>

<name>Drivers/BSP/STM32469I_EVAL/stm32469i_eval.c</name>

<type>1</type>

<locationURI>copy_PARENT1/Drivers/BSP/STM32469I_EVAL/stm32469i_eval.c</locationURI>

</link>

But if I want to create my own project I only can create a Linked Resource (FOLDER). If I edit the .project there are something like that:

<link>

<name>HAL</name>

<type>2</type>

<location>C:/workspace/SystemWorkbenchForSTM32/STM32F4xx_HAL_Driver</location>

</link>

<link>

<name>STM3246I_EVAL</name>

<type>2</type>

<location>C:/workspace/SystemWorkbenchForSTM32/STM32469I_EVAL</location>

</link>

How can I link a File Resource like does ST? (without editing the .project file) I can´t find this option in eclipse menus

Thanks in advance,

Sergio

1 ACCEPTED SOLUTION

Accepted Solutions
Posted on October 05, 2017 at 21:15

Hello Sergio!

You can add a Linked File Resource as below.

Right click to folder that you want to add the file  ->New->File.

Click 'Advanced' button.

Check  'Link to File in the File System'  checkbox.

Click button 'browse'

And choose the file you want.

Regards

vf

View solution in original post

4 REPLIES 4
Martin.Sergio
Associate III
Posted on October 05, 2017 at 11:23

I asked in System Workbench for STM32 Forum also

http://www.openstm32.org/forumthread5855

 

Still No Answer...

Posted on October 05, 2017 at 21:15

Hello Sergio!

You can add a Linked File Resource as below.

Right click to folder that you want to add the file  ->New->File.

Click 'Advanced' button.

Check  'Link to File in the File System'  checkbox.

Click button 'browse'

And choose the file you want.

Regards

vf

Posted on October 13, 2017 at 09:27

Hello,

  

Is it possible to add more than one file at a time?

Regards

   Sergio

Posted on October 13, 2017 at 23:00

Hello,

I don't know a way to choose many files and to  add at a time.

But by adding a folder, same way as file , adds also all the contents of the folder.

Regards.

vf