2013-07-26 12:54 AM
Hi,
I'm trying to sample a signal with the ADC and store data in the Micro Internal Flash. At the moment I sample the data with the ADC in continous mode and save the Data from ADC1_DR_Address with the DMA in RAM Area, but I need store more data. Is it possible that the DMA write it directly in Flash Area? I tried to save the data using ''FLASH_Status FLASH_ProgramWord(uint32_t Address, uint32_t Data);'' function but the time it takes to write the buffer is more time than it takes to fill completely. For example if my Ram Area is 70Kb i can save 70*1024/2 samples, and i fill that in 1 second (aprox I sample at 35Khz), but if I want to write 35K samples with FLASH_ProgramWord it takes arrond 1.25 seconds if I do so:/* Reset flags */
FLASH_ClearFlag(FLASH_FLAG_PGERR | FLASH_FLAG_WRPRTERR | FLASH_FLAG_EOP); /* Fill the flash buffer */ addr = (uint32_t)INIT
_FLASH_ADDR_DATA_REGION; FLASH_Unlock(); nw = TS_FLASH_size >> 2; for (i=0 ; i<nw ; i++) { status = FLASH_ProgramWord(addr, 2datasamples[i]); if (status != FLASH_COMPLETE) { FLASH_Lock(); /* Fail saving data */for(;;); } addr += 4; } FLASH_Lock(); so I can't record the Data when the interruption DMA_IT_HT of the DMA, occurrs. Is possible write in flash faster?? Best Regards,
2013-07-26 01:11 AM
Added More Info:
I'm using STM32F103RG (72Mhz Clock, 1MB Flash and 96Kb Ram) [STM32F10X_XL] ADC and DMA Config:SystemInit(); /* ADCCLK = PCLK2/8 */ RCC_ADCCLKConfig(RCC_PCLK2_Div8); /* Enable DMA1 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); /* Enable ADC1 and GPIOC clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_GPIOC, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; /* Configure PC.03 (ADC Channel13) as analog input */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; GPIO_Init(GPIOC, &GPIO_InitStructure); /* DMA1 channel1 configuration */ DMA_DeInit(DMA1_Channel1); DMA_InitStructure.DMA_PeripheralBaseAddr = ADC1_DR_Address; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)ADCConvertedValue; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize = MAX_SAMPLES; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1_Channel1, &DMA_InitStructure); /* Enable DMA1 channel1 */ DMA_Cmd(DMA1_Channel1, ENABLE); /* ADC1 configuration */ ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; ADC_InitStructure.ADC_ScanConvMode = ENABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); /* ADC1 regular channel13 configuration */ ADC_RegularChannelConfig(ADC1, ADC_Channel_13, 1, ADC_SampleTime_239Cycles5); /* Enable ADC1 DMA */ ADC_DMACmd(ADC1, ENABLE); /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE); /* Enable ADC1 reset calibration register */ ADC_ResetCalibration(ADC1); /* Check the end of ADC1 reset calibration register */ while(ADC_GetResetCalibrationStatus(ADC1)); /* Start ADC1 calibration */ ADC_StartCalibration(ADC1); /* Check the end of ADC1 calibration */ while(ADC_GetCalibrationStatus(ADC1)); SYSCLK/AHB Prescaler/APB2 Prescaler/ADC Prescaler/ADC_SampleTime 72Mhz/1/1/8/239=37Khz The Signal to Sample is a 10Khz signal --> ADC need Sample at 20Khz. Best Regards,
2013-07-26 03:36 AM
2013-07-26 04:15 AM
Thank you very much
I will try with a SPI External Flash