cancel
Showing results for 
Search instead for 
Did you mean: 

MB525 Eval Board CAN Issue

kaustubh
Associate II
Posted on January 07, 2011 at 22:35

MB525 Eval Board CAN Issue

1 REPLY 1
kaustubh
Associate II
Posted on May 17, 2011 at 14:20

Okay,

So here is the answer. This CAN setup cannot handle the speed with which data originates at the transmitter, meaning that the transmit mailboxes are full when subsequent iteration loops try to fill them up so packets are discarded. Adding a condition to check whether transmit mailboxes are empty or not and then transmitting solves the problem.

Thanks,

E