cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 @ 16Mhz TXCO

jaroslaw23
Associate II
Posted on March 08, 2011 at 21:38

STM32 @ 16Mhz TXCO

2 REPLIES 2
Posted on May 17, 2011 at 14:27

Yes this will work, you need to review the clock trees in the reference manual.

The USBCLK = PLLCLK/1 or PLLCLK/1.5, permitting a 48 MHz or 72 MHz SYSCLK for USB operation. You could also technically run the CPU at 8 or 16 MHz, and have the PLL just run the USB. The AHB, APBx can be a fraction of the SYSCLK.

The PLL can be driven by HSI/2, HSE, or HSE/2

An 6 or 12 MHz TCXO would also work.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jaroslaw23
Associate II
Posted on May 17, 2011 at 14:27

Thanks Clive,

I will write some more when I lunch the Project.