cancel
Showing results for 
Search instead for 
Did you mean: 

Stepper motor, 120Vdc, 6 Ampere

infoinfo983
Associate II
Posted on May 17, 2018 at 15:24

I would need advice on how to make a stepper motor drive with a supply voltage of 120Vdc and a current of 6 nominal Amps.

It seems to me there are only 2 ways, even if I do not know if they are feasible, they are:

1)

Use 2 PWD13F60 (2 H-bridges) to control the 2 windings of the stepper for the power part;

and use an STM32 microcontroller for the control part.

Sore point of this solution, I have not found any application notes that describe how to use the devices of the STM32 to directly control a stepper.

2)

Use 2 PWD13F60 (2 H-bridges) to control the 2 windings of the stepper for the power part;

and use an L6480 or L6482 controller for control.

Sore point of this solution, I do not know if the controllers that serve to directly drive the mosfet can be used only as 'digital' signals to drive the 2 H-bridges (which have already integrated the drivers).

Can someone help me on both questions or seal something else?

 

Thank you

0 REPLIES 0