cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F10x USB Virtual COM port driver for Linux ( ubuntu)

harinath
Associate III
Posted on August 18, 2013 at 07:32

Hi,

ST has driver for USB Virtual COM port for Windows. My STM32F10x devices works fine with that driver. I have just started working in Linux ( Ubuntu 12.04 LTS).

I'm having hard time in finding the USB virtual COM port driver for Ubuntu

I wonder do I also need to change the firmware part related to Virtual COM port for this !!

I appreciate if anyone points me in the right direction to accomplish this.

Thank you

#linux-driver
1 REPLY 1
zzdz2
Associate II
Posted on August 18, 2013 at 10:13

I'm not sure about Ubuntu but in Debian I haven't installed anything, it works out of the box.