cancel
Showing results for 
Search instead for 
Did you mean: 

IAR flash loader problem

cyril2399
Associate II
Posted on June 03, 2011 at 11:54

hello,

I'm working with the lastest version of IAR 6.203, and with a stm32F107 of the steval-pc010v1.

I want to load my program and IAr returns the attached file...

Is anyone have an idea for solving my problem?

Thanks to all

2 REPLIES 2
vikas_sinha75
Associate II
Posted on July 06, 2011 at 10:05

First of all check the connection and power supply if this is proper then you can check the memory location under options. If it doesnt work then you can try ''C:\Program Files\IAR Systems\Embedded Workbench *****bin'' and click on J-Link. it will reset some settings

Hope this will work

rosarium
Associate II
Posted on July 06, 2011 at 11:50

Just to check. did you copy the attached file intrinsics.h at the following path

C:\Program Files\IAR Systems\Embedded Workbench 6.0\arm\inc\c.

if yes then try as vikas said. Open the file jlink from C:\Program Files\IAR Systems\Embedded Workbench 6.0\arm\bin.

________________

Attachments :

intrinsics.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0ys&d=%2Fa%2F0X0000000biq%2F7JUK3paGXrc2AEAWCeASEr1YB8obk3UPNecs.9EyKzg&asPdf=false