2011-07-11 12:28 AM
Hello,
I have a stm3210C eval board and when I have launched it there was a program with sound, image, a game, web server all with icons. I have download an example program and now I it is the only thing I have on my eval board. I would like to found the first program that it had at the beginning. Where could I find it ? Thanks2011-07-11 12:40 AM
STM3210C-EVAL demonstration firmware at
http://mcd.rou.st.com/modules.php?name=mcu&file=familiesdocs&FAM=110#Firmware
2011-07-11 12:44 AM
http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/CD00237044.pdf
2011-07-12 12:19 AM
2011-07-12 01:21 AM
You are welcome... 🙂
2011-07-18 12:39 AM
Hello,
Into the firmware, the project ''DEMO'' has an empty main... the whole program is ''int main() {}''. I would like to see how it is programmed (icons, image player, system info etc...). Thank you2011-08-24 06:04 AM
Is there no way to have these codes?
2011-08-24 08:42 AM
Is there no way to have these codes?
It is no doubt using commercially licensed libraries, and you'd have to pay for them yourself. You should probably contact ST, or your FAE, to discuss the availability of source code, or portions thereof. I suspect supporting the application for everyone would tax the engineering resources available.