cancel
Showing results for 
Search instead for 
Did you mean: 

How program a new firmware without jtag linker

Posted on November 25, 2011 at 12:58

Is it possibile to program a firmware in a stm32f10x micro without a jtag linker?

Thanks in advance.
2 REPLIES 2
Posted on November 25, 2011 at 14:33

Is it possibile to program a firmware in a stm32f10x micro without a jtag linker?

They should also support the USART1 serial protocol using the system boot rom. Selected by the BOOTx pins. Others support CAN/USB modes. The protocol is described in several documents, there are ''Flash Loader'' applications.

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/CD00171488.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sbmeirow
Associate II
Posted on December 04, 2011 at 14:49

See

http://code.google.com/p/stm32flash/

 for programing flash in STM32 chips via UART (and RS232).

See

http://en.wikipedia.org/wiki/STM32#Development_tools

Steve Meirowsky

http://en.wikipedia.org/wiki/User:Sbmeirow