cancel
Showing results for 
Search instead for 
Did you mean: 

ACIM FOC library for STM32 ?

antonio239955_stm1_st
Associate II
Posted on November 13, 2017 at 22:26

Where to find the ACIM FOC library for STM32 ? When it will be in the STM32Cubexx ?

2 REPLIES 2
Amel NASRI
ST Employee
Posted on November 14, 2017 at 14:40

Hi

Cinelli.Antonio

‌,

Your request is transferred to our CubeMX who can decide if such request may be considered in new tool features.

Thanks for sharing.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Jeanne Joly
Senior III
Posted on February 15, 2018 at 10:36

Hello,

Are you aware of this library : 

http://www.st.com/en/embedded-software/stsw-stm32100.html

 ?

The STM32 PMSM FOC SDK(STSW-STM32100), which includes the PMSM FOC FW library and ST MC Workbench, allows the user to evaluate the STM32 performance in applications driving single or dual Field Oriented Control of 3-phase Permanent Magnet motors (PMSM, BLDC).

You can find the full description on Motor Control Software Development Kit in

http://www.st.com/content/ccc/resource/technical/document/user_manual/5e/5e/d2/cb/07/35/45/a6/CD00298474.pdf/files/CD00298474.pdf/jcr:content/translations/en.CD00298474.pdf

.

I am pretty sure it will help you.

BR. Jeanne