cancel
Showing results for 
Search instead for 
Did you mean: 

stm32w108cb - issue with TX in SimpleMac v2.0.1

maciej_zawodniok
Associate
Posted on November 24, 2014 at 20:10

Hi,

I'm using Dizic radio modules (STM32W108CB based ones) with SimpleMac v2.0.1 library.

Overall, the example projects work with exception of packet transmission (802.15.4). Every time it accepts the packet transmission with ST_RadioTransmit() but always ends with ''NO ACK'' case in callback function. Also, nothing is received in other modules (even in promiscuous mode).

I've tested it with XBee module and the STM32W/simplemac receives the packets from the XBee. But never transmits anything. No error but NO ACK is given.

#stm32w-wireless-simplemac
1 REPLY 1
Posted on November 24, 2014 at 20:33

There's really no support here for the STM32W108 devices.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..