cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F2XX Ethernet IAP

Asantos
Senior
Posted on December 06, 2011 at 15:31

I've tested the F2xx IAP over ethernet and it didn't work for me, the communications works okay, but the flash erase routine doesn't  work.

    Has someone tested this application?

3 REPLIES 3
amin23
Associate II
Posted on December 07, 2011 at 07:56

- check the STM32 EVAL jumpers setting

- which FW version you are using

- which protocol do you use http or tftp

Asantos
Senior
Posted on December 07, 2011 at 13:33

I'm using a custom board. I tried with both protocols. I noted that the erase flash function is called but it doesn't erase the flash.

This application worked for you?

amin23
Associate II
Posted on December 07, 2011 at 13:55

I am using ST EVAL, it works well.