cancel
Showing results for 
Search instead for 
Did you mean: 

Missing PWR_CR_PPDS definition in many L0 devices

Uwe Bonnes
Principal II
Posted on January 23, 2017 at 18:27

Hello,

e.g.  RM0377 lists the PWR_CR_LPDS bit unconditional for all L0X1 devices. * @version V1.7.1 headers define PWR_CR_LPDS only for L011 and L021. Is this right?

#stm32l0
1 REPLY 1
Amel NASRI
ST Employee
Posted on January 25, 2017 at 13:14

Hi

Bonnes.Uwe

‌,

In LPDS bit description in

http://www.st.com/content/ccc/resource/technical/document/reference_manual/21/bd/0f/bd/1c/88/40/f0/DM00108pdf/files/DM00108pdf/jcr:content/translations/en.DM00108pdf

, there is the following note: '

The LPDS bit is available on category 1 devices only'.

Category 1 devices are STM32L011xx & STM32L021xx (see table 1 in the reference manual).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.