cancel
Showing results for 
Search instead for 
Did you mean: 

Whats is Device Feature in dfuse ?

Uwe Bonnes
Principal II
Posted on May 01, 2017 at 15:57

E.g the F767 offers 4 dfu interfaces:

..  alt=3, name='@Device Feature/0xFFFF0000/01*004 e', serial='395734643435'

... alt=2, name='@OTP Memory /0x1FF0F000/01*001Ke,01*032 e', serial='395734643435'

... alt=1, name='@Option Bytes /0x1FFF0000/01*032 e', serial='395734643435'

... alt=0, name='@Internal Flash /0x08000000/04*032Kg,01*128Kg,07*256Kg', serial='395734643435

While I understand alternate interface 0-2, I don't find any information about the 'Device feature interface' . An3156 Table 6. mentions it as introduced with V2.1, but gives no further hint.

3 REPLIES 3
Uwe Bonnes
Principal II
Posted on May 05, 2017 at 11:22

Nobody has an idea?

Imen.D
ST Employee
Posted on May 08, 2017 at 14:08

Hi,

You may refer to the

http://www.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/12/1e/40/0c/CD00167594.pdf/files/CD00167594.pdf/jcr:content/translations/en.CD00167594.pdf

 (page 29) for more clarification.0690X00000606uPQAQ.png

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on May 08, 2017 at 14:56

Thnaks for the answer.

However the phrase 'device feature set' is no mentioned in section 3.4 'Bootloader Memory management' . I proposed to add the phrase 'device feature set' somehow in that section.