cancel
Showing results for 
Search instead for 
Did you mean: 

STCUBE offer 4-pin JTAG while erratta says: Full JTAG configuration without NJTRST pin cannot be used . .

Uwe Bonnes
Principal II
Posted on April 06, 2018 at 11:20

Hello,

I use stcube for pin allocation. At the moment I have a project with the STM32F303VD. The recent errata sheet clearly says: '2.1.3 Full JTAG configuration without NJTRST pin cannot be used .' However stcube offers a 4 pin JTAG entry. It would be helpfull, if stcube would gray out the 4 pin JTAG option for devices with the JTAG/NTRST errata so that people will not find out the errata later the hard way.

#tnrst-errata #stcubemx
0 REPLIES 0