cancel
Showing results for 
Search instead for 
Did you mean: 

ADC2_DMA_RMP[1] on STM32F334 (Rm0364)

Uwe Bonnes
Principal II
Posted on June 18, 2018 at 11:04

Hello,

as there is no DMA2 on the STM32F334, the SYSCFG->CFGR3 Bit 9 ADC2_DMA_RMP[1] has a misleading description. Following the description, is has to be kept set. 10.1.8 SYSCFG configuration register 3 (SYSCFG_CFGR3) is also missing Address offset and System reset value.

1 REPLY 1
Imen.D
ST Employee
Posted on June 19, 2018 at 11:20

Hello

Bonnes.Uwe

,

You are right, the description will be changed to:

Bit 9 ADC2_DMA_RMP[1]: ADC2 DMA controller remapping bit

0: Reserved

1: ADC2 mapped on DMA1

We will add the

missing Address offset and System reset value:

  • Address offset:

    0x50

  • System reset value:

    0x200

This is

rasied internally for update in the coming release of the reference manual RM0

With Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen