cancel
Showing results for 
Search instead for 
Did you mean: 

AHBxENR and AHBxLPENR

Uwe Bonnes
Principal II
Posted on January 06, 2015 at 11:06

Hello,

how is the relation between AHBxENR and AHBxLPENR? If some clock is disabled in run-mode, it is automatic also disabled in sleep mode despite the related LPENR bit _not_ reset?. Or is it needed explicit to reset the corresponding bit in the LPENR register to disable in sleep mode even so the corresponding bit is _not_ set  in run-mode?

I didn't find anything about this in several referenc manuals.

#ahbxerr #ahbxlpenr
0 REPLIES 0