cancel
Showing results for 
Search instead for 
Did you mean: 

Bad Phy strap values captured on Nucleo144 boards

Uwe Bonnes
Principal II
Posted on September 02, 2016 at 13:40

On one Nucleo-F746ZG and two NUCLEO-F767ZI boards, I have noticed that the captures strap values for Mode and Addr[0] often disaggree to the strapped values. The Phy LAN87xx requires the strap lines to be release at maximum 50 ns after NRST asserted. With NRST asserted on a running system, this requirement is probably not meet on the Nucleo144 boards.

I can resolve in two ways:

- Remove NRST <-> Phys RST Jumper SB 177 so that strap values only get captured with Power on reset with strap lines still in Hi-Z by the CPU so the resistor set strap value is not disturbed.

- Write Phy Register 18 lower byte to 0xe0 before giving a soft reset to the phy.
1 REPLY 1
slimen
Senior
Posted on September 05, 2016 at 11:47

Hi,

Thanks for sharing your solution.

Regards