cancel
Showing results for 
Search instead for 
Did you mean: 

STVP with Parallel Port Adapter Possible?

it2
Associate
Posted on August 09, 2011 at 23:23

Is it possible to use the STVP in a Windows XP environment with either a USB or PCI-e based ExpressCard Parallel Port adapter?  So far, I'm not having any luck as the software refuses to install the ParSTm driver because the parport service is not running.  The parport service won't start because it complains that it cannot find a device to use it with despite having correctly installed both of the previously mentioned adapters.

#driver #parallel-port #stvp
0 REPLIES 0