cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 RTC problem

Stephan Scherer
Associate II
Posted on May 02, 2018 at 14:51

Hello,

I have a problem. I use a STM32F427 with Keil RTX.

If I start my Programm without a backup battery my Programm runs into a rtos error (stack Overflow) if I want to set the date/time, but at this time the os isn't running.

I use an external 32768 Hz oscillator as LSE clock.

Can anyone give me a hint what I can do to solve this problem?

If I have a battery connected the Programm works fine at the second start, if there is a date/time in the system.

Best regards

Stephan

0 REPLIES 0