cancel
Showing results for 
Search instead for 
Did you mean: 

The I2C START BIT is not set after the I2C_generateStart

ihernandez
Associate
Posted on November 18, 2011 at 17:09

My I2C routines are found with stm32F103C6 but when I ' ve make a migration to STM32L my I2C routines are not foun.

The I2C START BIT is not set when I call the I2C_GenerateSTART(I2C1, ENABLE);

Anyone has been in the similar situation or issue?

Please I need any help..

I attach my I2C configuration:

ErrorStatus I2C_Start(void)

{

    if (I2C_State == I2C_S_INITING) return ERROR;

    if (I2C_State == I2C_S_STOPPING) return ERROR;

    if (I2C_State != I2C_S_STOPPED)

    I2C_State = I2C_S_INITING;

    /* I2C1 Periph clock enable */

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);

    GPIO_InitTypeDef  GPIO_InitStructure;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

    /* Enable APB1 I2C1 reset state */

    RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C1, ENABLE);

    /* Release I2C1 from reset state */

    RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C1, DISABLE);

    /* Enable the I2C EV Interrupt */

    NVIC_InitTypeDef NVIC_InitStructure;

    NVIC_InitStructure.NVIC_IRQChannel = I2C1_EV_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    /* Enable the I2C ER Interrupt */

    NVIC_InitStructure.NVIC_IRQChannel = I2C1_ER_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    /* I2C1 Init */

    I2C_InitTypeDef I2C_InitStructure;

    I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

    I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;

    I2C_InitStructure.I2C_OwnAddress1 = 0x00;

    I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

    I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

    I2C_InitStructure.I2C_ClockSpeed = 100000;

    I2C_Init(I2C1, &I2C_InitStructure);

    I2C_Cmd(I2C1, ENABLE);

    I2C_State = I2C_S_WAITING;

    return SUCCESS;

}

Also before the startgenerate call I make:

    /* Interruption enabled */

    I2C_ITConfig(I2C1, I2C_IT_EVT, ENABLE);

    I2C_ITConfig(I2C1,I2C_IT_BUF, ENABLE);

    I2C_ITConfig(I2C1,I2C_IT_ERR, ENABLE);

Thanks in advance,
1 REPLY 1
ihernandez
Associate
Posted on November 21, 2011 at 09:57

The issue is resolved.

I must to remap the pins SDA and SCL to the ports. In the STM32F plattform is not necesssary.

Bye everybody,