cancel
Showing results for 
Search instead for 
Did you mean: 

I/O Mirroring

jeffrey2399
Associate
Posted on September 26, 2016 at 16:23

I need to simply capture an input level and then output the same logic level as soon as possible on another pin.

This can be simply done with EXTI, but I was wondering if there is a passive peripheral based solution that could be done without software intervention.

I was wondering if one of the TIMERs could be re-purposed this way or some other peripheral?
2 REPLIES 2
Posted on September 26, 2016 at 17:33

Here we tend to use wire to achieve such effects.

TIM units would tend to divide (ie /2)

DMA doesn't really have the read/write functionality desired, and doesn't support bit-banding.

EXTI could be done quite efficiently.

What latency exactly are you looking for?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on September 24, 2017 at 08:42

Clive One wrote:

Here we tend to use wire to achieve such effects.

LOL @ dry British humour...

🙂