2011-09-27 11:20 AM
Hi,
I have a problem with the STM32VLDISCOVERY and IAR6.20. After Download and Debug I get the following: Loaded macro file: C:\Programme\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F10xxx.mac Fatal error: ST-Link Connection error Session aborted! Failed to load flash loader: C:\Programme\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F10xxxRAM6K.out Failed to load flash loader: C:\Programme\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F100xB.flash This only happens on my notebook computer, on my desktop everything is fine. I've already tried the ''um0892.zip'' trick, doesn't help. Any suggestions?2011-09-28 08:49 AM
2011-09-29 03:49 AM
Yap!
2011-10-03 09:52 AM
What is the fix, I am also seeing this problem. But not using SWD. Want to connect to the discovery kit.
2011-10-03 10:40 AM
What is the fix, I am also seeing this problem. But not using SWD. Want to connect to the discovery kit.
Unless I'm hopelessly confused, SWD is the only communication mode permitted by the ST-LINK on the VL-Discovery board. General advice : Make sure you have the most recent ST-LINK firmware. Make sure you have the most recent ST-LINK drivers, and that the tools can find and use this newer version over others it may have pathed/installed. Check the behaviour with ST-LINK the utilities. Call your IAR support representative.2011-10-03 10:13 PM
Hi,
looks lik it's a specific problem with my Lenove R500 ThinkPad Notebook. (...which so far works extremly well with any other software etc..) Using my old HP notebook everything works as expected. Furthermore, using the Lenovo together with an SEGGER JLINK EDU also woks fine, (JTAG as well as SWD). Of course I had to ''upgrade'' (in other words bypass the USB uC and piggy back a 20 Pin JTAG connector) the DISCOVERY a bit to do this test. Conclusion: For whatever reason the ST-Link and/or IAR stuff doesn't like my Lenovo or more likely some aspect it's XP installation - once again, greetings from Bill Gates. Hmmm....