cancel
Showing results for 
Search instead for 
Did you mean: 

USB2642 Power Draw

don239955
Associate
Posted on June 11, 2018 at 15:01

Hi,

I am trying to build a daughter card using the USB2642 to provide two USB ports and a SD card slot to a processor board.   I am trying to do a minimalistic design that draws the least amount of power and smallest foot print.   The daughter cards will be fixed.   I have created the following design and tested it and it works, but having a few problems:

1.  Power Draw, this board pulls 250mA of power with no SD card or USB devices attached and the USB2642 gets really hot.   Is this normal?    I don't believe it is so I am trying to figure out what wrong with my design.    Do I need EEPROM to change register values to control the FET? 

Also my USB cards are fixed and I tried power them from main power, and eliminate the MIC2026.  It didn't effect the power drain. 

Any thoughts?

#usb2642
0 REPLIES 0