cancel
Showing results for 
Search instead for 
Did you mean: 

CANopen stack SPEAr320

mirko239955
Associate
Posted on September 14, 2011 at 10:13

I'm looking for a CANopen software stack that can be implemented 

with the BSP running under Linux on SPEAr320,

for a project with a client  in the process automation.

Any software available from ST or 3rd parties ?

Thank you in advance

Mirko
5 REPLIES 5
hj
Associate II
Posted on September 17, 2011 at 22:25

Hello Mirko,

port GmbH at http://www.port.de offers a comercial CANopen stack which works with either can4linux or SocketCAN on Linux. Please check if one of these CAN drivers is available for the SPEAr320.

 

 Regards

    Heinz

hj
Associate II
Posted on September 17, 2011 at 22:29

Mirko

the exact link is

http://www.port.de/0564library

 Regards

    Heinz

mirko239955
Associate
Posted on September 19, 2011 at 12:02

Hi Heinz,

thank you for the infos.

i'm going to check it and come back to you asap.

Mirko 

myshanr
Associate II
Posted on January 14, 2012 at 07:42

表示看�懂,呵呵。怎么ST论�那么冷清的

翻译:I don't know, ha ha. How to ST BBS so cold

scott23
Associate II
Posted on May 22, 2016 at 13:18