cancel
Showing results for 
Search instead for 
Did you mean: 

DAC output buffer current sink specs

giu
Associate II
Posted on January 27, 2012 at 13:11

I can't find any info about the capability of the DAC output buffer of being a current sink. Is it possible? Which is the max sink current?

EDIT: I mean the DAC integrated on the uC chip and connected to GPIO pins, not the on board audio DAC
2 REPLIES 2
raptorhal2
Lead
Posted on January 27, 2012 at 16:37

Probably because the DAC output is a current source, not a a sink. If you really do mean sink, I am guessing it follows the same rules as any GPIO pin for current injection. If you mean source, Table 69 in the data sheet identifies the minimum load as 1.5K. If you mean current consumption, Table 69 gives quiescent current, to which you add the load current.

If this answer did not suffice, restate the question more specifically.

Cheers, Hal

giu
Associate II
Posted on January 30, 2012 at 13:01

I do mean current sink and not source. I already found the specification for the GPIO ports that you mention, but I wonder if the DAC pin has got different/better specs because of the software-selectable output buffer for analog signals.

Thanks for replying