2011-11-15 04:47 PM
#define SPI2_GPIO_CLK RCC_APB2Periph_GPIOB
#define SPI2_PORT GPIOB #define SPI2_CLK RCC_APB1Periph_SPI2 #define SPI2_SCK_PIN GPIO_Pin_13 #define SPI2_MISO_PIN GPIO_Pin_14 #define SPI2_MOSI_PIN GPIO_Pin_15 #define SPI2_NSS_PIN GPIO_Pin_12 #endif /* USE_SPI2 */ #define DUMMY_DATA 0x11 #define F_RAM_SPI_ID SPI2_ID #define F_RAM_PORT SPI2_PORT #define F_RAM_SCK_PIN SPI2_SCK_PIN #define F_RAM_MISO_PIN SPI2_MISO_PIN #define F_RAM_MOSI_PIN SPI2_MOSI_PIN #define F_RAM_NSS_PIN SPI2_NSS_PIN#define __SPI_HW__ 1
void SPI_Low_DeInit(void)
{ SPI_Cmd(SPI2,DISABLE); SPI_I2S_DeInit(SPI2); }void RCC_Configuration_SPI(void)
{ /*!< F_RAM_SPI_CS_GPIO, F_RAM_SPI_MOSI_GPIO, F_RAM_SPI_MISO_GPIO and F_RAM_SPI_SCK_GPIO Periph clock enable */ #ifdef USE_SPI2 RCC_APB2PeriphClockCmd(SPI2_GPIO_CLK | RCC_APB2Periph_AFIO, ENABLE); RCC_APB1PeriphClockCmd(SPI2_CLK, ENABLE); #endif}
void GPIO_Configuration_SPI(void)
{ GPIO_InitTypeDef GPIO_InitStructure; #ifdef USE_SPI2 /*!< Configure F_RAM_SPI pins: SCK */ #ifdef __SPI_HW__ GPIO_InitStructure.GPIO_Pin = SPI2_SCK_PIN | SPI2_MOSI_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(SPI2_PORT, &GPIO_InitStructure); #elif __SPI_SW__ GPIO_InitStructure.GPIO_Pin = SPI2_SCK_PIN | SPI2_MOSI_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(SPI2_PORT, &GPIO_InitStructure); #endif /* __SPI_HW__ */GPIO_InitStructure.GPIO_Pin = SPI2_MISO_PIN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; //GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(SPI2_PORT, &GPIO_InitStructure); /*!< Configure F_RAM_CS_PIN pin: F_RAM Card CS pin */ GPIO_InitStructure.GPIO_Pin = SPI2_NSS_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(SPI2_PORT, &GPIO_InitStructure); #endif /* USE_SPI2 */}
void SPI_Configuration(void) { #ifdef __SPI_HW__ SPI_InitTypeDef SPI_InitStructure; /*!< Deselect the F-RAM: Chip Select high */ //F_RAM_HOLD_HIGH(); F_RAM_CS(Bit_SET);#ifdef USE_SPI2
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; #if 0 SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; #else SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; #endif SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; #if 0 SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_16; #else SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; #endif #if 0 SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_LSB; #else SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; #endif SPI_InitStructure.SPI_CRCPolynomial = 7;SPI_Init(SPI2, &SPI_InitStructure);
/*!< Enable the sFLASH_SPI */
SPI_Cmd(SPI2, ENABLE); #endif /* USE_SPI2 */ #endif /* __SPI_HW__ */ }void main(void)
{
SPI_Low_DeInit();
GPIO_Configuration_SPI(); RCC_Configuration_SPI();SPI_Configuration();
}u8 F_RAM_SendByte(u8 byte)
{ u8 ret;/*!< Loop while DR register in not emplty */
while (SPI_I2S_GetFlagStatus(F_RAM_SPI, SPI_I2S_FLAG_TXE) == RESET);/*!< Send byte through the SPI1 peripheral */
SPI_I2S_SendData(F_RAM_SPI,(u16)byte); /*!< Wait to receive a byte */ while (SPI_I2S_GetFlagStatus(F_RAM_SPI, SPI_I2S_FLAG_RXNE) == RESET);/*!< Return the byte read from the SPI bus */
ret = (u8)SPI_I2S_ReceiveData(F_RAM_SPI); return ret; } ===============================================================2011-11-15 05:16 PM
2011-11-15 05:46 PM
change RCC and GPIO.
but not active spi2. schmetic is ...