cancel
Showing results for 
Search instead for 
Did you mean: 

SPI BSY erratum listed under I2C in 'F76x/77x errata

Posted on February 07, 2017 at 14:29

In STM32F76xxx and STM32F77xxx silicon limitations DocID028806 Rev 4, 2.2.2  BSY bit may stay high at the end of a data transfer in slave mode which is entirely an SPI error, is listed under I2C peripheral limitations.

JW

1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee
Posted on February 07, 2017 at 16:16

Hi Jan,

Thanks for keeping this error to our attention: I confirm that the limitation 'BSY bit may stay high at the end of a data transfer in slave mode' is misplaced and should belong to SPI limitations.

This is noted and will be fixed in next errata version.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Amel NASRI
ST Employee
Posted on February 07, 2017 at 16:16

Hi Jan,

Thanks for keeping this error to our attention: I confirm that the limitation 'BSY bit may stay high at the end of a data transfer in slave mode' is misplaced and should belong to SPI limitations.

This is noted and will be fixed in next errata version.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.