2014-12-15 12:11 AM
Thanks to Mayla for updating us. Again, it's a pity the announcement is locked and we can't discuss the merits of the new STM32 family members...
Some remarks to the text in the announcement: - SPDIF is Rx only, if I understood right - the 7 I2S channels are to be read as 3 simplex I2S shared with 3 SPI, plus 2 duplex I2S - QUAD-SPI (YES way to go, ST!) - it's not ''dual'' as ''two pieces'', but as ''dual mode'' - can work ''normally'' through registers, but also through memory mapped acces (way to go, again!) - LCD support - it's just a marketing fluff, if I understood correctly, it means ''you can attach a display with controller supporting 8080/6800-style interface, through FMC'' - 180MHz system clock - the strange combination of peripherals hints a strong customer with particular requirements ... 😉 Btw. anybody noticed this is the first even-numbered STM32F4? 🙂 JW