cancel
Showing results for 
Search instead for 
Did you mean: 

Bootloader for STM32F0 and STM32F3

Frank Voorburg
Associate II
Posted on November 15, 2016 at 18:12

Today I released version 1.2.4 of the open source OpenBLT bootloader. It now features support for both the STM32F0 and STM32F3 family of microcontrollers, in addition to the STM32F1, STM32F2 and STM32F4, which were already supported.

I added demo programs for the Nucleo-F091RC and Nucleo-F303K8 boards. Using the demo programs for these Nucleo boards, you can perform firmware updates via UART and CAN.

Download is available from https://www.feaser.com

Feedback and ideas are always welcome!

-Frank

#bootloader #openblt
1 REPLY 1
slimen
Senior
Posted on November 15, 2016 at 18:23

Hello,

Thanks for this sharing. It should be helpful.

Regards