cancel
Showing results for 
Search instead for 
Did you mean: 

What's the difference into SDCARD with SD_CD pin or not with?

esiqueira
Associate II
Posted on July 04, 2013 at 02:16

And how should I configure this pin?

MISO is Input Pull Up

CLOCK and MOSI are Alternate Function Push Pull 

CS is Output Push Pull

and CD is ???????????

#sdcard-spi-cd-cs-mosi-miso-clock
1 REPLY 1
Posted on July 04, 2013 at 03:10

CD = Card Detect

Usually a switch like structure in the socket/slot, to indicate the presence, insertion, removal, or lack of card.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..