cancel
Showing results for 
Search instead for 
Did you mean: 

USB mass storage with Linux and OS-X

hli2
Associate II
Posted on November 12, 2009 at 07:04

USB mass storage with Linux and OS-X

2 REPLIES 2
hli2
Associate II
Posted on May 17, 2011 at 13:29

Hi everybody,

Does anybody try to use the USB mass storage system under Linux and OS-X environments ?

In our case, the first trials do not work properly. The OS see the structure of the media but after that, nothing is working properly. For example, the data files retrieved from the media is full of 0.

Any comment is welcome as we are lost in our analysis.

Best regards,

HLI

g-ab
Associate II
Posted on May 17, 2011 at 13:29

Hi hli,

I am using USB mass storage, demonstration with Linux(2.6.5) and STM3210E-EVAL board, to read/write sdcards.

attached is a short log.

>> SD card file system is FAT32''

regards,

G.Ab.

[ This message was edited by: g-ab on 12-11-2009 11:38 ]