cancel
Showing results for 
Search instead for 
Did you mean: 

DMA pheripheral transfer example

abhishek2
Associate II
Posted on August 18, 2008 at 09:45

DMA pheripheral transfer example

2 REPLIES 2
abhishek2
Associate II
Posted on May 17, 2011 at 12:42

HEllo everybody

I am stuck with building the DMA example 4 in which the ADC (pot in STM3210B-EVAL board) is configured to generate PWM pulses at the output (PA08) through the DMA channel5. I am able to build the project and even download it into the flash. Unfortunately I do not see any change in the Oscilloscope. The debug does not end with highligting the int main function which usually happens with other examples. Only ''break'' and ''stop debugging'' buttons are active and others are inactive in IAR.

Thanking you

AR

16-32micros
Associate III
Posted on May 17, 2011 at 12:42

Hi,

May this link helps you :

http://www.st.com/mcu/forums-cat-7180-23.html

Cheers,

STOne-32.