cancel
Showing results for 
Search instead for 
Did you mean: 

Discovery BaseBoards (for F4, F3, and VL)

kornak
Associate II
Posted on February 20, 2013 at 03:50

I have made baseboard PCBs for the Discovery-F4, Discovery-F3 and Discovery-VL that break out the signals to separate connectors for various ports and interfaces.  

I am offering the PCBs for sale if you would find them helpful for a project.

Photos, schematics, and BOM links are available on my blog:

http://kornakprotoblog.blogspot.ca/2013/02/four-stm32-discovery-baseboards.html

Has anyone seen any other baseboards or expansion boards for the STM32 Discovery modules?

1. I have links to the Embest STM32F4DIS-BB Ethernet baseboard for the Discovery-F4 on that page.

2. Gage submitted a link (on Hackaday.com) to the wvshare.com Open-407-IC board which is very interesting.  Search for Open407 on eBay, or take a look at this link:

http://www.wvshare.com/product/Open407I-C-Standard.htm

It does not use the Discovery-F4 module, but it comes with a similar module.

#discovery-f4-stm32-f3-vl
1 REPLY 1
Posted on February 20, 2013 at 04:41

It does not use the Discovery-F4 module, but it comes with a similar module.

An arguably better board in fact, using the 176 pin LQFP instead of the 100 pin one, and not cluttered with other circuitry.
Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..