cancel
Showing results for 
Search instead for 
Did you mean: 

Pinout Spreadsheet for the STM32F4-Discovery Available

kornak
Associate II
Posted on January 05, 2012 at 18:47

I have created an Excel spreadsheet to help in the Discovery-F4 pin assignment process, and as a useful reference for the pin functions. 

The STM32-Discovery-F4 pinout spreadsheet lists the Discovery modules pin information along with the alternate functions available for each pin.  This spreadsheet helps me to plan my projects by assigning pin names and rearranging the rows to group related pins.  I have color coded the pin functions to help me see what functions are available on which pins.

Details are available at:

http://kornakprotoblog.blogspot.com/2012/01/pinout-spreadsheet-for-stm32f4.html

I hope you find the spreadsheet to be helpful for your projects.

The spreadsheet can be downloaded from

http://kornak.ca/parts/stm32-discovery-f4/

http://kornak.ca/parts/stm32-discovery-f4/

.

Updates to this spreadsheet will be available in this directory when they are released. 

Revision 1.00 is named ''Kornak-(STM32-Discovery-F4)-0001 Rev 1.00 Module Pinouts & Functions.xls''

I would appreciate any comments or suggestions you may have on the spreadsheet. 

Please send them to

mailto:kornak.busboard@gmail.com

or add them to this discussion thread.

#stm32f4-discovery #stm32f4
3 REPLIES 3
elijah
Associate II
Posted on January 07, 2012 at 08:40

Thanks, Scot. Useful spreadsheet. I guess it's not a bad idea to publish that on Google docs, it will be a bit more useful on-line.

serggorsky
Associate II
Posted on September 13, 2012 at 03:54

Thank you for a great tool, it really helped me to integrate several breadboard sketches to one solid project.

BTW, I don't see any advantage of making the doc online. Since it's project-based, the right place for it is the project folder on the disk. imho. 🙂
kornak
Associate II
Posted on October 02, 2014 at 18:18

Due to changes to the

http://kornak.ca

web site, we have to move the STM32-Discovery-F4 pinout spreadsheet to our

http://busboard.com

. It is now with the other documentation for our

http://busboard.com/pcb-stm32-f4b1

for the Discovery-F4 module.

The spreadsheet can be downloaded from 

http://busboard.us/products/PCB-STM32-F4B1/

 .  Updates to this spreadsheet will be available in this directory when they are released.  

Revision 1.01 is named ''

http://busboard.us/products/PCB-STM32-F4B1/Kornak-%28STM32-Discovery-F4%29-0001%20Rev%201.01%20Module%20Pinouts%20%26%20Functions.xls

''

I've received many emails from people saying the spreadsheets and baseboards have been useful for their projects.  Thanks!

Here are the updated links to the Discovery module baseboards currently available:

http://busboard.com/PCB-STM32-VLB1

http://busboard.com/PCB-STM32-F3U

http://busboard.com/pcb-stm32-f4b1

http://busboard.com/KIT-BB2-F3-F4

Schematics and BOMs are available for the baseboards.

Cheers!

Scot Kornak