2012-02-02 05:30 AM
Greetings,
I am currently toying around with the KEIL MCBSTM32F200 Evaluation Board(the STM32F207VG uC) and have run into some problems with the PWM output.I want a simple PWM-signal on TIM1, Channel1 (PA8 for STM32F205&207) usingthe standard peripheral library for STM32Fxx.The code below is a mix from the different examples from the standardperipheral library examples for PWM, and I'm sure something critical ismissing.After initializing, all TIM1 registers looks ''ok'' (as far as I can tell, thetimer is a bit too advanced for me...) and the TIM1_CNT register is countingup and resetting.When connecting the oscilloscope to PA8, all I get is a steady 3.3V signal,no PWM.What am I missing here? It's quite frustrating since all other peripheralsI'm using are working fine. Thanks in advance.(code also at : http://pastebin.com/yUmZbXUL)&sharpinclude ''stm32f2xx.h''&sharpinclude ''stm32f2xx_gpio.h''&sharpinclude ''stm32f2xx_rcc.h''&sharpinclude ''stm32f2xx_tim.h''&sharpinclude ''system_stm32f2xx.h''/****************************************************************************/void main(void) { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; GPIO_InitTypeDef GPIO_InitStructure; uint16_t period; uint16_t pulse; /* Initialize clock - defined in system_stm32f2xx.h */ SystemInit(); /* Compute the value for the ARR register to have a period of 20 KHz */ period = (SystemCoreClock / 20000 ) - 1; /* Compute the CCR1 value to generate a PWN signal with 50% duty cycle */ pulse = (uint16_t) (((uint32_t) 5 * (period - 1)) / 10); /* GPIOA clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* Initialize PA8, Alternative Function, 100Mhz, Output, Push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1); /* TIM1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 , ENABLE); /* Timer Base configuration */ TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = period; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* Channel 1 output configuration */ TIM_OCStructInit(&TIM_OCInitStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = pulse; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OC1Init(TIM1, &TIM_OCInitStructure); /* TIM1 counter enable */ TIM_Cmd(TIM1, ENABLE); /* TIM1 Main Output Enable */ TIM_CtrlPWMOutputs(TIM1, ENABLE); /* forever... */ while (1) { __asm(''nop''); }} #stm32f2xx-pwm-tim12012-02-02 09:22 AM
Your duty computation seems overly complicated. I'd compute the period value, program the period-1 into the timebase, and period/2 for 50% into the the pulse.
The SystemInit() stuff is called by the C startup code prior to main(), at least in my environment. I don't have your board/chip. Here is an example for TIM4, Channel 1, out of PD.12 on a STM32F4-Discovery. Doing this on a STM32F2 should be a matter of changing the clock prescaler computation.// STM32 PWM STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* TIM4 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
/* GPIOD clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOD, &GPIO_InitStructure);
/* Connect TIM1 pins to AF */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_TIM4);
}
/**************************************************************************************/
void TIM4_Configuration(void)
{
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
uint16_t Period;
Period = 1000000 / 20000; // 20 KHz for 1MHz prescaled
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Prescaler = ((SystemCoreClock / 1000000) / 2) - 1; // Get clock to 1 MHz on STM32F4
// TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // Get clock to 1 MHz on STM32F2
TIM_TimeBaseStructure.TIM_Period = Period - 1;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
/* Enable TIM4 Preload register on ARR */
TIM_ARRPreloadConfig(TIM4, ENABLE);
/* TIM PWM1 Mode configuration */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50%
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
/* Output Compare PWM1 Mode configuration: Channel1 PD.12 */
TIM_OC1Init(TIM4, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Enable);
/* TIM4 enable counter */
TIM_Cmd(TIM4, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
TIM4_Configuration();
while(1); // Don't wait to exit
}
/**************************************************************************************/
2012-02-02 09:35 AM
This should be a workable TIM1 CH1 PA.08 implementation
// STM32 PWM (TIM1 CH1 PA.08) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* TIM1 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);
/* GPIOA clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect TIM1 pins to AF */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1);
}
/**************************************************************************************/
void TIM1_Configuration(void)
{
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
uint16_t Period;
Period = 1000000 / 20000; // 20 KHz for 1MHz prescaled
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // Get clock to 1 MHz on STM32F2/F4
TIM_TimeBaseStructure.TIM_Period = Period - 1;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
/* Enable TIM1 Preload register on ARR */
TIM_ARRPreloadConfig(TIM1, ENABLE);
/* TIM PWM1 Mode configuration */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50%
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
/* Output Compare PWM1 Mode configuration: Channel1 PA.08 */
TIM_OC1Init(TIM1, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable);
/* TIM1 Main Output Enable */
TIM_CtrlPWMOutputs(TIM1, ENABLE);
/* TIM1 enable counter */
TIM_Cmd(TIM1, ENABLE);
}
/**************************************************************************************/
2012-02-03 02:35 AM
Thanks for the reply! Problem solved 🙂
The missing function call is:TIM_OCxPreloadConfig(TIMx, TIM_OCPreload_Enable)
Buried in stm32f2xx_tim.c there is a note:Note2: In case of PWM mode, this function is mandatory:<
br > TIM_OCxPreloadConfig(TIMx, TIM_OCPreload_ENABLE); However, in the 7PWM_Output example for the library, this function is not called (and there is no PWM output on any pins). Also, the word ENABLE should not be upper-case. For posterity, a fully functional snippet for a single PWM on PA8, TIM1 (with a bit too complicated period/pulse calculation):#include ''stm32f2xx.h''
#include ''stm32f2xx_gpio.h'' #include ''stm32f2xx_rcc.h'' #include ''stm32f2xx_tim.h'' #include ''system_stm32f2xx.h'' /****************************************************************************/ void main(void) { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; GPIO_InitTypeDef GPIO_InitStructure; uint16_t period; uint16_t pulse; /* Initialize clock - defined in system_stm32f2xx.h */ /* May not be needed */ SystemInit(); /* Compute the value for the ARR register to have a period of 20 KHz */ period = (SystemCoreClock / 20000 ) - 1; /* Compute the CCR1 value to generate a PWN signal with 50% duty cycle */ pulse = (uint16_t) (((uint32_t) 5 * (period - 1)) / 10); /* GPIOA clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* Initialize PA8, Alternative Function, 100Mhz, Output, Push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1); /* TIM1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 , ENABLE); /* Timer Base configuration */ TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = period; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* Channel 1 output configuration */ TIM_OCStructInit(&TIM_OCInitStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = pulse; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OC1Init(TIM1, &TIM_OCInitStructure); /* Very much needed. Enable Preload register on CCR1. */ TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable);/* TIM1 counter enable */
TIM_Cmd(TIM1, ENABLE); /* TIM1 Main Output Enable */ TIM_CtrlPWMOutputs(TIM1, ENABLE); /* forever... */ while (1) { __asm( ''nop'' ); } }2012-02-15 11:10 PM
Hi Tomas,
have you tried to using a different pin? I tried your's code and it works, but when I changed the Pin_8 to Pin_7 it doesn't work. GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; -> GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1); -> GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_TIM1); And of course I tried also other Pins 12 and 10. Same case: only pin 8 works. I don't understand it. Could you test your's board, please?2012-02-16 02:39 AM
Hi Tomas,
forgot about my previous message. I didn't understand how ports and pins mapping together with timers.2014-03-22 02:00 AM
Hi Clive1
I'm replying to your very old post because I have a problem with my stm32f4discoveryboard (407vt chip onboard) specific with TIM4. It is mapped to PD11..14. Whatever I try I can not get PWM signals on the 4 channels.I found your code, it looks almost like mine but I copied it anyway. I get some strange 50Hz like noise signal on my scope and superimposed on it I see (using your code) a very tiny 500mV PWM wave. Now when I configure TIM3 for PWM (same mode pwm1) I get nice pwm signals.I'm totally puzzled about it....Do you perhaps have an idea or suggestion what this might cause? The discoveryboard has 500ohm resistors with a LED connected to ground but that cant be it right?CheersDennis2014-03-22 08:21 AM
Yeah, that doesn't sound right, but I don't have a scope to hand right now.
I did build a 4-channel servo demo for the STM32F4-DISCO using the LED pins, you could try that.2016-07-18 08:10 AM
2016-07-18 08:32 AM
Can we please STOP cross-posting into multiple old threads. You should have opened a new one initially.