cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F107 SPI3 Remap

mvonahnen
Associate III
Posted on January 23, 2015 at 18:55

Can some of the pins of a peripheral be remapped while others stay at their existing AF location?  I noticed in reference code on the STM32F107 that appears that some of the pins are remapped, but not all of them.

I want to dynamically remap the SS pin for SPI3 to drive two devices, can this be done without moving the MISO, MOSI, and SCLK pins?
1 REPLY 1
Posted on January 23, 2015 at 19:18

What does the Reference Manual suggest?

Drive the Chip Select as a GPIO, then you can use any pin(s) you want.
Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..