cancel
Showing results for 
Search instead for 
Did you mean: 

MicroXplorer as Eclipse plugin with Linux

Moritz M
Associate II
Posted on May 31, 2012 at 12:27

Hi,

does anybody use the MicroXplorer Eclipse plugin with Linux and Eclipse 3.7?

Here it either crashes Eclipse or I can't choose an MCU.

Moritz

#microxplorer-ubuntu64-crashes
3 REPLIES 3
colignya3
Associate II
Posted on September 06, 2012 at 23:06

Mine also cannot operate,

using Ubuntu 64 with Eclipse Indigo,

the following eclipse.ini at least and at last got me opening all:

-startup

plugins/org.eclipse.equinox.launcher_1.2.0.v20110502.jar

--launcher.library

plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.1.100.v20110505

-showsplash

org.eclipse.platform

-vm

/usr/lib/jvm/java-7-oracle/jre/bin/java

--launcher.XXMaxPermSize

2048m

--launcher.defaultAction

openFile

-vmargs

-Xms128m

-Xmx2048m

All else is well.

 

But if I stretch the MicroXplorer menu open, it crashes.

[I pull the separation bar up so that the blue MicroXplorer icon get larger]

Before it crashes - I also cannot select MCU's

I tried everything I could find on the net.

[I did install everything the proper way]

Tired, Desperate...

colignya3
Associate II
Posted on September 07, 2012 at 08:34

System

It is an Intel MB, 16Gig RAM, Quad Processor

Nvidea graphics

colignya3
Associate II
Posted on September 07, 2012 at 08:35

UBUNTU error report:

The crashed program seems to use third-party or local libraries:

/home/za/eclipse/plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.1.100.v20110505/eclipse_1407.so

/home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-gtk-3740.so

/home/za/eclipse/configuration/org.eclipse.osgi/bundles/84/1/.cp/os/linux/x86_64/libunixfile_1_0_0.so

/home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-atk-gtk-3740.so

/home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-pi-gtk-3740.so

/home/za/eclipse/configuration/org.eclipse.osgi/bundles/271/1/.cp/libswt-cairo-gtk-3740.so

It is highly recommended to check if the problem persists without those first.

 

What do I do with this?