cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32L-DISCOVERY and WITH Keil MDK Light V4.23

carl239955
Associate II
Posted on February 18, 2012 at 18:08

I am able to open, compile and download both supplied projects from ST for the STM32L-DISCOVERY Framework. When running in DEBUG mode when the debugger excecutes the function Icc_run() at about line 221 in the AN3413 Current consumption.......... I get a STLinkIII error message ''Internal command error'' then ''Error  attempting to read 64bytes  from 0x00000000''

Any help will be appreciated.

0 REPLIES 0